Hi
Now I using TDC1000 Webench tool to Calculated expected time-of-flight (TOF), but I have some question as below.
1. Does the Distance need to add the object thickness?
Ex: If the object thickness is 2mm & internal width of the object is 100mm then distance need to define 100mm or 102mm?
2. How can to define the distance to 50mm through Webench Tool? Current only setup to 0.1m as below.
3. What meat is the "% Change in Medium"?
Thanks your help.