Hi --
I am using the TDC7200 in a simple application that reads a single STOP signal within a range of about 100ns - 125us. I am having trouble getting the INT_MASK, STOP_MASK, and overflow registers set properly.
I want to signal INTB as soon as the measurement is complete, but it always delays until either COARSE or CLOCK overflows occur, depending on the overflow value I set. Using INT_MASK 0x01 seems like it should set "interrupt on measurement only", but it still waits for an overflow.
What are the proper register settings to have the TDC complete a measurement and set INTB right after the first STOP pulse, without waiting for overflows?
Thanks!
John