This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC 1612 no read after shutdown



Hello,
I have ldc 1612 for Inductive Sensing.
I'm using NI cRIO with LV 2015 to create the I2C communication. 
I succeeded to create the communication and get reads from the ldc 1612. but after i shut down the device (by entering High at the sd input) and turn on again (entering Low at the sd input) and try to get read from the channels (o or 1) i always get 0. However when i insert 0X7F\0X7E command i get the correct read.
I tried to to use the config command (0X1A4001) and other configuration but didn't succeeded.
What can i do? 

Thanks From ahead 

Tamir