I’m looking to develop a mass-produced consumer product that can externally measure the fill level of a tank using your ultrasound technology. There are a couple of criteria the product would have to meet to be successful.
1) The ultrasound would have to penetrate steel of about 5mm thickness and measure a fill level varying from about 2cm to about 50cm.
2) It should be possible to measure the fill level of different tanks with the same product without too much difficulty, i.e. the transducer isn’t adhered to the tank.
Do you think your TDC1000 component could be suitable for this application?
Thank you