Hi,
I have one question about Spring Inductance measure method, now the Spring parameter as below.
Diameter = 5.9 mm
Number of Turns = 13
Height = 24 mm
How can to Calculate the Spring inductance?
Now use LCR meter to measure the inductance that it is 2.2uH.
Would you kindly share the Spring design application note for our reference?
Thanks.