This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ultrasonic B-Scan

Other Parts Discussed in Thread: TDC1000, TDC7200

Hi all, silly question here.

I made up a first revision of a PCB of project where i use TDC1000 and TDC7200 ICs, i'm planning to use it to measure water temperature in a non invasive way based on the ToF.

But after some searching i found a couple of videos where a ultrasonic transducer is used to generate images of the surface of the Device Under Test, based on the A-Scan information.

Some of the videos of the TDC1000-TDC7200 EVM seems to show a kind of A-Scan, do you think it is possible to generate a "primitive" B-Scan, or even a "primitive" C-Scan (3D images) based on the ToF calculated by the TDC7200 in conjunction to the TDC1000.

All opinions are welcome :)

Thanks in advance