This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How much maximum operable temperature of HDC1080

Other Parts Discussed in Thread: HDC1080

Hello,

I want to make industrial wireless temprature and humidity sensor using TI HDC1080.

May I know what is maximum temperature range it can measure?

I am looking for chemical and energy industry where temperature goes 250*C or more can it measure that much or any other sensor of TI can do this?

Thanks

Regards

Abhishek

  • Hi Abhishek,

    With the HDC1080, the temperature range that can be measure is from -40 to 125°C.

    For temperaure sensor that works at higher temperature you can take a look to the LM95172-Q1, that works until 200°C, but if you need more information about it, please refer to the temperature sensor forum:

    Best regards,

    Carmine