Hello Team,
I was looking into the HDC1080, and had a question regarding as to how relative humidity is measured relative to temperature.
My understanding is that %RH is measured as a ratio between the pressure of the waver vapor at a specific temperature, and the max quantity of water vapor that the air can hold at that specific temperature. As seen in the snaa216 app note equation (1):
Is this consistent with how the device determines the %RH, and if not is there any compensation that needs to be done?
Best Regards,
Javier Palomo