Hello,
I want to use a telescopic antenna as proximity sensor with FDC2x14.
My requirements:
- detection of human hand at up to 50-100cm distance
- the digital value read from the sensor should reflect the distance from the antenna, so it's rather a distance measurement than a presence detection
To check if it's possible, maybe someone can help me with the following questions:
- I've a FDC2114EVM, so the sensor resolution is 12 bit. The FDC2214 has 24 bit resolution. Should I use the FDC2214 instead for those requirements? If yes, can I simply replace the device on the EVM and the EVM microcontroller and the GUI software will work correctly or do I have to buy the FDC2214EVM instead? On a first look, the firmware of the microcontroller is the same for both devices.
- According to application notes, the LC tank capacitor should be as small as possible. If I reduce the capacitor value on EVM and increase the inductor value, would this help to increase the range and the sensitivity?
- If I understand the sensor types correctly, I should use the single ended configuration. So, the antenna reference is earth. This means, the circuit GND must be connected to earth, right?
- Which register settings have most effect on range and sensitivity? It seems that there's no software tool which goes through the different combinations automatically to figure out the best results.
Thanks a lot for comments and suggestions.
Regards,
Ralf