I would like to know if it is possible to create an LVDT with only one secondary coil?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello James,
something similar has been done here: http://www.ti.com/lit/an/snoa931/snoa931.pdf
Thank you Ben for your reply. I am trying to simplify what we make now. The primary coil is divided in two coils running in series and the secondary is in two different locations with it's own primary. We use small pieces of metal to balance the coils which can be time consuming. What I would like it so be able to eliminate one of the secondary coils and maybe use a circuit or chip to act as the secondary coil. Is there such a thing?
James
Hello James,
an MCU is required to configure the device and read the data. I recommend looking at an MCU with integrated DAC if you need an analog output.
Hi Ben,
Thank you for your information. I would need a MCU with integrated DAC for the LDC10101 as well as voltage regulator that will drop from 12VDC to the voltage that is needed. These will need to be mounted on a circuit board that would be about 1 inch round. What MCU would you recommend?
Regards,
James
Hello James,
for questions on low-power MCU selection, please post your requirements in the MSP forum; my colleagues from the microcontroller team will assist: http://e2e.ti.com/support/microcontrollers/msp430/
Ben,
Can the component circuit board that has the LDC1101 chip be stacked on top of the circuit board coil? If so, how close can they be before interfering with readings.
Also, the capacitor for the coil, does it have to be next to the coil or can it be with the LDC1101 chip if the LDC1101 chip is in close proximity to the coil?
We are looking to use this as analog out with a reading of 0V - 5V. What is the resolution output? Can it detect less than .003" change?