This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to do the Nonlinearity Calibration voxel viewer



Hello,

I'm trying to make a non-linear calibration. I put an obstacle in front of the camera and through the watch list I get the phase and the measured distance by me. The ​​phase range is from 200 to 2500, how should I put them inside the box of calibration? Because I can set the Phase period 90°, 180° or 360°.

With these data I have to perform a task before inserting them into the look up table?

Thanks