This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

set saturation_threshold in the configuration file OPT9221 in OPT8241 voxel viewer ToF ( saturation threshold )



Hello,

I'm trying to change the saturation threshold  through voxel viewer for a particular profile (which is associated its own .conf configuration files) but I can not do it. I have tried to add it manually in the configuration file but it does not appear to have any changes. Reading the pdf of the OPT9221 says : Saturation flag is set if the ambient value of the pixel is lesser than or equal to this value. Also, pixel phase data is set to 000h. How can I do?

Anyone can help me?

Thanks