In the description of the OPT8241-CDK-EVM, it is said the operating range of the EVM is up to 4m.
My question How far is the operating distance limitation of the TOF Camera designed with OPT8241/OPT9221? & what is The depth resolution of the system with OPT8241/OPT9221?
What is the Key factor of the system design for the operating distance? LED components, lens, or noise effect?