Good morning to all,
I just bought a EVM for test the FDC2214.
I need some advice on how to connect the three signals: SD - INTB – ADDR.
If i want a fixed address, can i connect the ADDR signal for example to GND ?
In what manner, directly or with a resistor?
If i do not want to manage the SD signal I have to connect it to what potential (+3.6 volts or GND)?
In what manner, directly or with a resistor?
The same thing for the signal INTB
Thank's in advance
Whisky