Dear Technical Support Team,
I have a question about FDC2214.
Do you have some information of external amp for shield?
What type of opamp do you recommend?
Datasheet shows below, but it doesn't have the detail.
----------------
in order to minimize interference from external objects, some applications require an additional plate which acts
as a shield. The shield can either be:
• actively driven shield: The shield is a buffered signal of the INxA pin. The signal is buffered by an external
amplifier with a gain of 1.
-------------------
Regards,
ttd