My potential application of TI TOF sensor requires very high frame rate.
I used OPT8241-CDK-EVM with Voxel Viewer.
To get high frame rate I started with No Calibration Profile in Voxel Viewer, which automatically set
dealias_en=False, mod_freq1=48MHz and quad_cnt_max=4.
I changed sub_frame_cnt_max to value of 1.
To decrease readout time, I set ROI to 320 by 1.
Then voxel Viewer changed Video Mode to 120 fps.
After that I manually increased fps until Voxel Viewer showed Error “Failed to set frame rate at 241.00fps” and crashed.
What is the reason for limiting fps to 240?
By the way, the real frame rate was not 240 fps but 200 fps, as can be seen on the attached oscillogram of emitted laser light.