I'm using 2 LM95234 in a switch design where 1 is connected to 4 MMBT3904 and the other to 4 internal diodes of a Broadcom BCM54680 Phy.
The one with the MMBT3904 works perfectly but the one connected to the broadcom PHY's don't give any values. The MSB register just have the sign bit set and the software shows -128 on all channels. I've gone trough all registers and there's no hint why this happen. The fault register is clear and the chip is converting.
I've tried many options strting from the default values and also changing the diode model but without success. In a former design the Phy's are working well with an on ADT7461 Temperature sensor. Does anyone have an idea what have gone wrong or have the same experience?