Hey!
I am designing PCB coils for LDC1612. The WEBENCH tool gives me the capacitor value of 24.9pF. And the BOM list gives me a capacitor with value of 22pF. May I know if this is critical?
At the same time, I am using axial sensing technique for distance sensing. Do I need to calibrate the sensor with micrometer or some other tools before actual application?
And last question is, is there a way to properly mount the PCB coil and the metal target? To avoid interference, I guess I cant use screws to mount them. So do people usually mount the PCB coil and metal target with glue? Is there a way to properly align the PCB coil axis with the round metal target central axis?
Thank you!