Hi,
I am currently working with the FDC1004EVM board. I have cut appart the original sensors and I have connected a home made sensor. Now, the pins CIN1, SHLD1 and SHLD2 are connected to some cooper electrode.
When I try to connect the FDC1004EVM board, the red LED is ON and no connexion is made (the GUI display "no connect"). Sometimes, when I touch the output pins while connecting the device, the green LED turns ON and I am able to speak to the device with the GUI.
I have seen somewhere that maybe the MSP430 turns the red LED when the sensor is detected as "not the original one". That wouldn't be problematic if I was still able to communicate with the device, which is not the case.
Do you see any explanation why this would happens, and how to fix it?
Thank you for your time, I hope I was able to be clear enough...
Vincent