Hello,
I want to do a distance measurement using the TDC1000, TDC7200 and an ultrasonic sensor. The measurement range is between 65 mm and 375 mm.
Is it possible to achieve a resolution of 10 µm or less with this setup?
I only saw the reference design from TIDA00322, which doesn´t use the TDC7200.
I would appreciate your help.
Kind Regards