This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about LM75A reading cycle

Other Parts Discussed in Thread: LM75A

hi dear supporting team,

in LM75A d/s, there is description on the temperature reading cylce requirement, which is max 300ms over temp  and 100ms at room temp.  customer want to know whether we have the temp curve VS reading cycle requirement?   in higher or lower temp it will request longer cycle to read? 

(the background of the question is: customer did not notice the 300ms requirement when they design the brd, and the make it 244ms, now it seems hard to change the s/w version and need ship out 450pcs brds soon, they want to know the rule of our chip, so they can do some temp experiment on the brds to see the worst case.They agree to change the reading cycle later)