This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ultasonic transducer for metal thickness

Other Parts Discussed in Thread: TDC1000

Dear Sirs


I need to measure the thickness of metal 10-50mm and was thinking about ultrasconic sensors.

Do you know if there is a fairly inexpencive transducer that can do this and also survive G-forces and chock movements?

Best

/Dan

  • TDC1000 is targeted for liquid level measurements and liquid/gas flow measurements. Sorry we don't have suggestion/experience on a ultrasonic transducer for metal thickness. Thanks, Vishy
  • EM2210 Pocket-size Thickness Gauge EMAT (Oktanta-NDT) oktanta-ndt.ru/.../ 2 - 60 mm +/-0.05 mm , ultrasonic thickness gauges (not represented on the site. Manufactured by "Oktanta-NDT" but under a different trademark) - from 2 to 200 mm. EM2210 , EM1301 , Measurements can be taken without usage of couplant, without advance surface preparation and across the operating gap between the transducer and the test object of up to 3 mm