This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: TDC7200 abuout the time issue and the enable pin issue

Part Number: TDC7200

Hi Team,

The customer is using TDC7200. He has two issues.

Q1.: For example, after a Start signal is sent, theoretically, the Stop signal is needed to sent 5 times, but  in fact, the Stop signal is only sent one time.

Then the TDC7200 device will continue to wait for the following Stop signals.  

How does the TDC7200 device know when it  stops waiting  the following Stop signals?

Q2: After power up (VDD supplied, ENABLE Pin low to high transition), the internal registers are initialized with the

default value. 

Are the default value for the internal registers the RESET VALUE of Table 1. Register Summary in the datasheet?

Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments