Hello,
I was hoping to find a product or set of products that are capable of sensing speed and direction of a rotating object. I am not looking for a specific technology, only that it can meet my requirements. However, I am looking for the sensor and the object it will be tracking (for instance, a hall effect sensor and the magnet disk being sensed, or a inductive sensor and the gear with the teeth being sensed). I tried contacting the chat on the website who instructed me to contact semiconductor customer support who instructed me to contact the forum.
I prefer a sensor with:
- Two channels at a 90 degree phase shift and a 50% duty cycle
- A speed range of 0-15000 rpm and 32 to 80 pulses per revolution
- A unit width of 6.2mm and a shaft diameter of the disk of 15mm to 45mm.
These are the specs I am looking for, but please show me any available options.
Thank you in advance