This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1314DIAL-EVM: EVM "Not Connected" to GUI

Part Number: LDC1314DIAL-EVM
Other Parts Discussed in Thread: LDC1314

Hello,

I have LDC1314DIAL-EVM, I have installed the 1.9.1 version of Sensing Solutions EVM GUI, and I have the firmware .txt file for the ldc1314 sitting on my desktop.

When I start the GUI then plug in the EVM the device status says "Not Connected" and to the right of that reads "Ready" . Windows detects the EVM as COMx (where x is 4,5,6, etc). The device LEDs turn on Red for D3, green for D2.

When I plug in the EVM then start the GUI the device status says "Not Connected" and to the right of that reads "SSP EVM Disconnected". Windows detects the EVM as COMx (where x is 4,5,6, etc). The device LEDs turn on Red for D3, green for D2.

I have tried pushing firmware (even though it says the device is not connected), the loading bar runs forever, and I have to exit and restart the GUI.

I have tried reinstalling the GUI.

I have tried reinstalling the drivers from Windows for the EVMs.

I found a similar post on this topic but the answer there did not resolve my issue: e2e.ti.com/support/sensor/inductive-sensing/f/938/t/554277 

Thanks,

Nick