Other Parts Discussed in Thread: HDC1010,
Hi Team,
The customer will use HDC1080 and HDC1010 in a magnetic field environment.
Q1: The customer needs to know if there are the internal crystal oscillators for these two devices.
Q2:If there are the internal crystal oscillators for these two devices, are the crystal oscillators signals done shielding measures inside of the two chips? Does the customer need to consider the EMC problem in practical applications for the two devices?
Q3: The customer needs to know if the IIC signals and the internal AD be easily influenced by the magnetic field environment.
If the IIC signals and the internal AD can be easily influenced by the magnetic field environment, how to solve the issue?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments