This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241-CDK-EVM: OPT8241-CDK-EVM USB device not recognized

Part Number: OPT8241-CDK-EVM

The board did work a couple times, but not reliably. Now it always fails to connect on USB. I am using Windows 10, and a 5V 3A power supply. When I plug the device into the Windows computer, the computer shows a dialog with "USB device not recognized", and the device manager indicates an error.