Other Parts Discussed in Thread: TMP006
Hi:
I've been using TMP006EVM on object temperature measuring , found that the measured temperature is far lower than the actual object temperature and beating more than 10 ℃.Picture 2 and 3 pictures shows development board from 7mm object to be tested,the Objects at 54 ℃ however TMP006EVM measured results is only about 40 ℃ and jumping from 36℃ to 49℃, how can I improve the measurement precision and reduce the jitter,thanks!
Best Regards,
TongSiPu
Hardware engineer