This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8 channel 2.5 nanosecond beamforming system.

I’m looking buy or build a system that can receive eight sinusoidal signals from 1 MHz up to 10 MHz, delay each channel with a set delay (minimum of 2,5ns and max 2,5us with steps of 2.5ns), combine them (sum or sum/avg) and send the combined (analogue) signal out again. This system should preferably be analogue, but if it must internally be digital the sampling rate should be sufficient to exclude under-sampling.

I would like to know if anyone has experience with something near to this or if anyone know a company that sells a product like this?

  • Hi Jelle,

    The ultrasonic devices covered in this forum do not have the functionality you are searching for. I am not sure which group has something that matches your requirements. You will have to do some searching on the forum to find the correct one.

    Thanks, and good luck,