Part Number: TMP007
Hi Sir,
What's the maximum temperature that tmp007 can sense? Could it be used to sense 150 ℃ object and what about the accuracy. If not, does TI have another device that can perform contactless temperature sensing? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMP007
Hi Sir,
What's the maximum temperature that tmp007 can sense? Could it be used to sense 150 ℃ object and what about the accuracy. If not, does TI have another device that can perform contactless temperature sensing? Thank you.
We have data showing the TMP007 measurement precision +/-3C in the object temperature range +25C....+300C with parts calibration. The precision can be even better if the object temp. calculation would be done outside the device or object temp range is reduced.. The through hole mounted method was used and via was covered with capton tape to lower the IR signal intensivity.