This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDC1000-TDC7200EVM: TDC1000-TDC7200EVM

Part Number: TDC1000-TDC7200EVM

Tool/software: TI C/C++ Compiler

hello guys i am using msp430f5528 micro controller. now i need to interface my microcontroller with lcd 16x2 display (4 bit mode). i am using TDC1000-TDC7200EVM. i have connected RS, RW, E to P4.2, P4.4, P4.5 respectively and i have connected D4, D5, D6, D7 (MSB) to PJ.0, PJ.1, PJ.2, PJ.3 respectively. i need to display "hello world" in lcd display in 4 bit mode. i want the embedded c program for that. can anyone please code and give to me ? asap.