This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT70A: Multiple Sensor Input with Decoder

Part Number: LMT70A


I'm trying to read multiple sensors with a single precision ADC, but I don't know if my designs are correct. The idea is to expand the number of temperature sensors (32 LMT70A) that a microcontroller with a limited number of analog ports can process. The datasheet mentions that enable pin allows multiple sensors to share one ADC channel and when T_ON is set to a logic "LOW" the TAO pin is set to a high impedance state. The following schematic shows how I was planning to build the circuit, but for now only with four sensors.

Are there any special considerations I must follow? Are there any other components I need to place on the circuit?