Other Parts Discussed in Thread: LDC1314, LDC1312
Hi Team,
My customer considers to use LDC2114 for angular position sensing like the following application note.
http://www.tij.co.jp/jp/lit/ug/tidu953/tidu953.pdf
He wants to use LDC2114 as substitute for LDC1314 because his application requires space limiting and low power (battery powered).
Is it possible to use LDC2114 for angular position sensing?
I believe it is possible to read DATAn by I2C (not to use OUTx pin in this case).
If the answer is yes, I would like to ask if it is achieved by only 1 channel or 2 channels because application note use 4 channels of LDC1312.
He want to achieve more than two angular position sensing by one device (LDC2114).
Best Regards,
Yaita / Japan disty