Part Number: OPT8241-CDK-EVM
I recently received an OPT841-CDK-EVM and had it working. In looking at some of the recommendations, I updated the TFC firmware using the OPT9221_0v26.tie file from the TI website. Now I can connect to the board but the imaging is not working and the TFC LED does not illuminate. The Master LED is bright green. When connecting with Voxel Viewer v0.9.6, I get the following messages in the log:
Voxel Viewer v0.9.6
Texas Instruments Inc.
INFO: TintinCDKCamera: Board revision = 2.0
INFO: ParameterDMLParser: Found register map with name 'OPT9221' (vPG1P0)
INFO: HardwareSerializer: Received 45755 bytes from hardware in 2.06034 s
INFO: Data2DCodec: Original number of 8-bit offsets = 3101
INFO: Data2DCodec: Number of invalid pixels in original data = 0
INFO: Data2DCodec: Current number of 8-bit offsets = 3101
ERROR: DepthCamera: Could not set the camera profile to '111'
ERROR: DepthCamera:Could not get value for parameter TintinCDKCamera(0::0451:9105::10408871039087).vco_freq1
ERROR: DepthCamera: Failed to update value for parameter 'mod_freq1'
ERROR: DepthCamera:Could not get value for parameter TintinCDKCamera(0::0451:9105::10408871039087).vco_freq2
ERROR: DepthCamera: Failed to update value for parameter 'mod_freq2'
ERROR: DepthCamera: Failed to update value for parameter 'sysclk_in_freq'
ERROR: DepthCamera: Failed to update value for parameter 'quad_cnt_max'
ERROR: DepthCamera: Failed to update value for parameter 'vco_freq2'
ERROR: DepthCamera: Failed to update value for parameter 'vco_freq1'
ERROR: DepthCamera:Could not get value for parameter TintinCDKCamera(0::0451:9105::10408871039087).vco_freq1
ERROR: DepthCamera: Failed to update value for parameter 'mod_freq1'
ERROR: DepthCamera:Could not get value for parameter TintinCDKCamera(0::0451:9105::10408871039087).vco_freq2
ERROR: DepthCamera: Failed to update value for parameter 'mod_freq2'
ERROR: DepthCamera: Failed to update value for parameter 'sysclk_in_freq'
ERROR: DepthCamera: Failed to update value for parameter 'quad_cnt_max'
ERROR: DepthCamera: Failed to update value for parameter 'pixel_data_size'
ERROR: DepthCamera: Failed to update value for parameter 'output_mode'
ERROR: DepthCamera: Failed to update value for parameter 'vco_freq2'
ERROR: DepthCamera: Failed to update value for parameter 'vco_freq1'
ERROR: CameraSystem: Could not refresh parameters for TintinCDKCamera(0::0451:9105::10408871039087).
ERROR: DepthCamera:Could not get value for parameter TintinCDKCamera(0::0451:9105::10408871039087).vco_freq1Traceback (most recent call last):
File "C:\Anand\Work\Code\voxel-viewer\build\VoxelViewer\out00-PYZ.pyz\PyVoxelViewer.docks.FrequentlyUsedParametersDockWidget", line 93, in updateView
File "C:\Anand\Work\Code\voxel-viewer\build\VoxelViewer\out00-PYZ.pyz\PyVoxelViewer.docks.FrequentlyUsedParametersDockWidget", line 46, in showParam
File "C:\Anand\Work\Code\voxel-viewer\build\VoxelViewer\out00-PYZ.pyz\PyVoxelViewer.views.ParameterHandlerROI", line 127, in __init__
File "C:\Anand\Work\Code\voxel-viewer\build\VoxelViewer\out00-PYZ.pyz\PyVoxelViewer.views.ParameterHandlerROI", line 259, in init
File "C:\Anand\Work\Code\voxel-viewer\build\VoxelViewer\out00-PYZ.pyz\PyVoxelViewer.views.XYSpinBox", line 35, in setRange
OverflowError
CalibrationStatus: Calibration invalid for - Temperature.
ERROR: ToFCameraBase: Could not get current frame rate
INFO: ToFCameraBase: Starting with 456x456@0fps
ERROR: TintinCDKCamera: Could not get current frame rate