Part Number: AFE5807EVM
Other Parts Discussed in Thread: AFE5807, CDC7005, AFE5809
I am developing a system using the AFE5807 and currently I'm using the EVM and the ADC<->HSMC adapter card. It seems like the EVM has to be set up by the windows software to make the clock circuit work properly. Is there a way to do this setup through the HSMC adapter card instead? (I guess SPI cs for the CDC circuit must be available on the HSMC) Having to first boot into windows to set up the EVM and then boot back to my regular development environment is not an ideal solution.
-Øystein-