This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5812: ADC sampling rate

Part Number: AFE5812
Other Parts Discussed in Thread: AFE5818EVM

Hello,

The AFE5812 has ADC with stated sampling rate of 65 MSPS at 14-bit.

1. Is it per channel or for all channels?

2. If it's for all channels, can I assume that it would be 65/8 = 8 MSPS per channel?

3. Can I get a higher sampling rate at 12-bit?

4. Is the digitalized data only accessible via LVDS?

Thanks.