This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM: Exporting Time of Flight Value

Part Number: TDC1000-C2000EVM


I am using the TDC1000-C2000EVM for a level sensing application. From this data, I want to be able to do additional numerical transformations and check these values against certain logical constraints. To do this, I want to be able to import the values from the provided by the TI GUI into LabVIEW. I know that on the TDC1000-TDC7200EVM there is an option to export the calculated value using UART stream. Is there a way to do this using the TDC1000-C2000EVM, perhaps using NI's VISA interaction? I also have a NI DAQ with 250Ks/s resolution if there is a way to externally interface with the board to get the value of the TOF. Any help would be greatly appreciated.