Checking with the experts on if there is a reference design for an Electromagnetic Water Flow Meter.
These are also known as Magmeters.
A magnetic field is created using motor type circuit and when energized the voltage is measured across the interior of the flow meter body.
The voltage is measured in on both cycles of the fields as they alternate and when combined and divided by 2 much of the line noise is removed.
These flowmeters are highly accurate.
If there isn't a public application then are TI resources available for a private design?