This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM26LV-Q1: Behavior when VDD level is lower than VTEMP level

Part Number: LM26LV-Q1


Hello Champs,

 

I have question when 2.5V voltage is supplied to LM26LV-Q1 Gain 4 option device.

When ambient temperature is low, how VTEMP output behave?

According to Table 1. VTEMP OUTPUTVOLTAGE vs. DIE TEMPERATURE graph, VTEMP output is 2.651V at DIE temperature is 0C.

Can I think VTEMP output is just clamped around 2.5V, and in the range where DIE temperature is high, device operates normally?

Best regards