Other Parts Discussed in Thread: MSP430F5529, , TDC7201, TDC7200EVM, TDC7200
Hello,
I am working to construct a range finding system using TDC7201-ZAX-EVM and MSP430F5529.
I installed TDC720xEVM and its related firmwares and confirmed the above combination worked.
Now, I would like to customize TDC720xEVM for my system. I have two questions.
1. Is it possible to have a LabVIEW source file of TDC720xEVM?
2. The evaluation board of TDC7201 is seen as TDC7200 (com6) from the device manager. I tried to access the evaluation board using terminal programs (like Teraterm or simple Labview program for serial communication), however, I could not have meaningful response from the board. I sent some commands according to "host_interface.h" in a demo project TDC7200EVM_USB, however, it did not work. It is very kind of you to provide me with tips to communicate with TDC7201. GUI source file will be also very helpful to understand this question.
Thank you for your kind consideration.
Best regards,
Shunsuke Kono