This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443: Matlab error using RadarStudio PostProc

Part Number: AWR1443

Hi,

I am having issue with the Matlab PostProc GUI that reports an error when I try to process my captured data. It appears that there is some problem with the data structure as it does not match the expected dimensions. Below is the console output printing the error message.

[RadarAPI]: ar1.StartMatlabPostProc("C:\\Program Files (x86)\\Texas Instruments\\RadarStudio\\PostProc\\adc_data.bin")
[10:23:47]  [RadarAPI]: Error: 
[10:23:47]  
[10:23:47]  ... MWMCR::EvaluateFunction error ... 
[10:23:47]  Array dimensions must match for binary array op.



I kept most of the default settings, but did make some changes. Below are the changes made:

  • ChannelConfig: Enabled TX1 and RX1. Single Chirp
  • LVDS Lane Configuration: Format 0. LVDS Lane1, Lane2, Lane3, Lane4 enabled. MSB First
  • Frame: 32 frames