tried to connect CCS with new received AWR1443 EVM, but failed, so is AWR1642 EVM.
When I tried to connect to R4F, it always asks me to update the XD110 firmware as attached. If I clicked update, the CCS will hang.
I also tried to update the XDS110 firmware in command line. After I ran xdsdfu.exe -m, there's still no XDS110 com ports under Device Manager
This is warning message:
Warning:
A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target.
DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE.
(Emulation package 6.0.579.0)