Hello, I have an application where there is a spinning disk with targets on it and the distance from the target can be 0.25" to 0.5" at a speed of 400rpm. What is the minimum distance and maximum speed that the IWR1443 can support?
Thank you!
David