Hey guys,
I need to find a solution to measure the time between two fast spinning pulleys. I consider to get the signal from a photodiode or a hallsensor. Need to check which one is better.
My smaller pulley is running with round about 1600hz. In combination with the tooth I get 25600Hz for both pulleys. I need to measure a time difference between the two signals in a range of 5ns.
Would this be possible with the TDC? And what others components do I need for this.
Is the signal that comes from a photodiode or hallsensor already suited for the TDC?
Would it be possible to save the data constantly over a longer period of time(minutes)?
I am a total beginner and dont have really a clue about this stuff.
Need more informations?
Thanks for your help.
Pascal