Other Parts Discussed in Thread: AWR1243
Hello everyone
In this white paper. it said that "TI’s radar chip includes a built-in digital frequency shifter to frequency-shift the samples, perform image-reject filtering and send out the complex baseband output at the reduced interface rate (similar to a real-only implementation)." Can you tell me where can I find this digital frequency shifter on the chip?
Another question, as mentioned in the document "The band-pass IF chain has configurable lower cutoff frequencies above 350 kHz and can support bandwidths up to 15 MHz. ", which means any frequencies below 350KHz would be filtered out. This does not make sense, because the low beat frequencies in the close range detection will be filtered. Can you tell me why?
Thanks
Peter