Other Parts Discussed in Thread: AWR1443, UNIFLASH, , AWR1243
I'd like to set AWR1642EVM to use under combination of BoostPack+DevPack+TSW1400. I got advice below...
• you will find AWR16xx firmware binary at ‘mmwave_dfp_00.06.01.01\firmware\mss\ar16xx’ which you can use with RadarStudio to send CMD over SPI.
• When you are using RadarStudio with AWR16xx you need download only BSS and MSS binaries in SOP2 mode, no need to download config file.
• AWR16xx firmware provided in this DFP 00.06.01.01 version can be used only in SOP-2 mode.
• With AWR16xx you need to use ‘ar1xxx_bss_rprc.bin’ fw file to download to the device from ‘mmwave_dfp_00.06.01.01\firmware\bss’ path.
• On AWR1443 this version of DFP won’t work, you need to use DFP 00.06.00.05 version.
But I could not flash ‘ar1xxx_bss_rprc.bin’ file to AWR1642EVM as below.
***Uniflash log ***
[2017/5/26 3:30:58] [INFO] CortexR4_0: Initialization complete.
[2017/5/26 3:30:58] [INFO] CortexR4_0: Flashing process starting...
[2017/5/26 3:30:58] [INFO] CortexR4_0: Connecting to COM Port COM7...
[2017/5/26 3:30:58] [INFO] CortexR4_0: Reset connection to device
[2017/5/26 3:30:59] [INFO] CortexR4_0: Set break signal
[2017/5/26 3:30:59] [INFO] CortexR4_0: Connection to COM port succeeded. Flashing can proceed.
[2017/5/26 3:30:59] [INFO] CortexR4_0: Reading device version info...
[2017/5/26 3:30:59] [INFO] CortexR4_0: ** 2 files specified for flashing.
[2017/5/26 3:30:59] [INFO] CortexR4_0: Checking file C:/ti/mmwave_dfp_00.06.01.01/firmware/bss/ar1xxx_bss_rprc.bin for correct header for AWR1642.
[2017/5/26 3:31:00] [INFO] CortexR4_0: Header of C:/ti/mmwave_dfp_00.06.01.01/firmware/bss/ar1xxx_bss_rprc.bin file indicates it is not a valid file to flash to AWR1642: 0x43525052
[2017/5/26 3:31:00] [ERROR] CortexR4_0: !!! Aborting flashing of specified files!!!
[2017/5/26 3:31:00] [INFO] CortexR4_0: Disconnecting from device on COM port COM7...
[2017/5/26 3:31:00] [INFO] CortexR4_0: Flashing instance clean-up initiated...
[2017/5/26 3:31:00] [INFO] CortexR4_0: Instance deinitialized!
************