This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP007: TMP007: Spec and implementation question

Part Number: TMP007


Can you comment on the below questions?

1.       Is the TMP007 sensor max maximum range 10mm (from data sheet).

2.       Can this sensor can be glued. If so which glue is more preferred. Please confirm.

3.       Is there any preferred orientation to mount sensor?

 

Thanks!