This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDC1000-TDC7200EVM: I want TDC1000-TDC7200EVM Driver or I want example project for Interfacing SPI.

Part Number: TDC1000-TDC7200EVM

Tool/software: Code Composer Studio

Hi,

Please read my query,

I am working with TDC1000-TDC7200EVM and Interfacing SPI with some another micro controller(xx family).

What I need is I want driver/component for TDC1000.

Actually I am working with Keil IDE.

So, I need a driver lib for total TDC1000 with SPI protocol.

Please anyone knows suggest me.

Thank you,

Regards,

Vivek

  • Hello Vivek,

    Included with the TDC1000-TDC7200EVM GUI is the full firmware for use with the MSP430 on the EVM board. No other libraries have been developed, but the firmware can provide examples for how the SPI communication is done with the MSP430 and serve as a starting point for other platforms.

    It is located in the following folder once the GUI is installed: C:\Program Files (x86)\Texas Instruments\TDC1000_7200EVM\Firmware

    Regards,