Other Parts Discussed in Thread: AWR1243, UNIFLASH
Hi,
We have the three board combo of the eval boards AWR1243BOOST + MMWAVE-DEVPACK + TSW1400.
We have been able connect to AWR1243 and XDS1010 does show up as to different COM ports.
The serial flash on AWR1243BOOST has been erased and two firmware bin files in DFP package have also been loaded via the uniFlash Tool.
Then we connected the mmwavedevpack board to the 1243boost, and also connected the USB to the computer. The mmdevpack gets recognized as four unknown devices in device manager. Then we updated
the drivers on these 4 unknown devices using the ftdi drivers in DFP package. All the four unknown devices now show up as USB serial bus controllers and not as COM ports as we expected. I believe this may also be the reason why we cant connect to the two boards via Radar Studio.
Look forward to your help on this.
Regards,
RJ