Part Number: OPT8241-CDK-EVM
Hi,
I have a few questions regarding methods in which this TOF camera will fail.
- Say one of the applications is a real-time analysis of a dark object on a conveyor belt, how fast can the conveyor belt be moving before errors become large?
2. How dark of a material can be used before not enough infrared light is reflected back to the camera? Does texture play a role in this? (assume a working distance of ~2m)
3. How shiny of a material can be used before too much light is reflected back? Does texture play a role in this? (assume a working distance of ~2m)
4. Is the TOF Camera/software able to distinguish between different objects or materials? If so, how does it do this? Ex. a bin full of sand; can the bin and the sand be distinguished from one another? What if the bin and the sand are the same color?
5. Is the TOF Camera/software able to create a depth map of a pile of big rocks? Or would occlusions become too big of a problem?
6. How bright and clear of an image is possible with different combinations of working distance and Field of View?
Thanks,
Sabrina